deEmbed De-Embeds an adapter or multiple adapters from a 2-port
measurement. All S-Parameter inputs must be aligned. Port 2 of
one network feeds port 1 of the subsequent network (see diag).
This fuction supports de-embedding of adapters on either side
of the DUT. If only a single adapter is used, set unused
adapter to [] or repmat([0,1;1,0],[1,1,num_pts])
_______________________________________
| _______ _______ _______ |
A_DUT_B o-|---|P1 P2|---|P1 P2|---|P1 P2|---|-o A_DUT_B
Port1 | | S_A | | S_DUT | | S_B | | Port2
o-|---|_______|---|_______|---|_______|---|-o
|_______________________________________|
S_dut = deEmbed(S_A_DUT_B,S_A,S_B)
inputs:
S_A_DUT_B: [2,2,num_pts] S-Parameter description of the combined
network Adapter A - DUT - Adapter B
S_A : [2,2,num_pts] S-Parameter description of adapter on
the left (Port 1) side of the DUT
S_B : [2,2,num_pts] S-Parameter description of adapter on
the right (Port 2) side of the DUT
outputs:
S_dut: [2,2,num_pts] S-parameter description of the DUT